AXIS#.MOTOR.VOLTRATED

Description

This parameter configures the drive for the induction motor's rated voltage as indicated on the nameplate.

AXIS#.MOTOR.VOLTRATED is used to calculate the constant Volts per Hertz characteristics of the drive and motor.


  • This parameter is required to be configured for AXIS#.MOTOR.TYPE = 2.

Context

For more information see Motor.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

V

Range

50 to 1,000 V

Default Value

230 V
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
AXIS1.MOTOR.VOLTRATED

500bh

06h

Unsigned16

-

-

Read/Write

No

AXIS2.MOTOR.VOLTRATED

510bh

06h

Unsigned16

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.MOTOR.VOLTRATED

6226

1852

Unsigned16

Read/Write

-

AXIS2.MOTOR.VOLTRATED

71762

1185

Unsigned16

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.MOTOR.VOLTRATED

6226

Unsigned16

Read/Write

-